cancel
Showing results for 
Search instead for 
Did you mean: 

ADC using DMA works in 8-bit mode even though a resolution of 12-bit is activated.

fiona_io
Associate

Hello,

I would like to use an ADC using DMA in 12-bit mode. 

Unfortuntaly, the adc value is only 8-bit which doesn't match with my configuration. I've already tried to solve the problem by trying the solution proposed here: https://community.st.com/t5/stm32-mcus-products/why-would-an-adc-sample-in-8-bit-mode-when-dma-is-used-but-when/m-p/197276/highlight/true#M42484

But it didn't work in my case.

Here's my source code for dma and adc. I am not working with the cubeIDE anymore, that's why my configuration functions look different than the auto-generated init-functions of the IDE. The weird thing is that the same configuration is working in the CubeIDE... (so maybe it's a structual problem in my configuration)

 

ADC_HandleTypeDef hadc1;
DMA_HandleTypeDef hdma_adc1;

uint16_t buffer;
uint16_t adc_value;

 void DMA1_Channel1_IRQHandler(void) {
   HAL_DMA_IRQHandler(&hdma_adc1);
 }

void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc) {
   adc_value = buffer; //store value
}

void adcInit(void) {
  GPIO_InitTypeDef GPIO_InitStruct = {0};
  RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
  ADC_MultiModeTypeDef multimode = {0};
  ADC_ChannelConfTypeDef sConfig = {0};
  __HAL_RCC_ADC12_CLK_ENABLE();
  PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_ADC12;
  PeriphClkInit.Adc12ClockSelection = RCC_ADC12CLKSOURCE_SYSCLK;

  if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK) {
    Error_Handler();
  }

  __HAL_RCC_GPIOC_CLK_ENABLE();

  /**ADC1 GPIO Configuration
  PC2     ------> ADC1_IN8
  */

  GPIO_InitStruct.Pin = GPIO_PIN_2;
  GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

  hadc1.Instance = ADC1;
  hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV2;
  hadc1.Init.Resolution = ADC_RESOLUTION_12B;
  hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
  hadc1.Init.GainCompensation = 0;
  hadc1.Init.ScanConvMode = ADC_SCAN_DISABLE;
  hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
  hadc1.Init.LowPowerAutoWait = DISABLE;
  hadc1.Init.ContinuousConvMode = DISABLE;
  hadc1.Init.NbrOfConversion = 1;
  hadc1.Init.DiscontinuousConvMode = DISABLE;
  hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
  hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
  hadc1.Init.DMAContinuousRequests = DISABLE;
  hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
  hadc1.Init.OversamplingMode = DISABLE;

  if (HAL_ADC_Init(&hadc1) != HAL_OK) {
    Error_Handler();
  }

  /** Configure the ADC multi-mode */
   multimode.Mode = ADC_MODE_INDEPENDENT;

   if (HAL_ADCEx_MultiModeConfigChannel(&hadc1, &multimode) != HAL_OK) {
     Error_Handler();
   }

  /** Configure Regular Channel */
  sConfig.Channel = ADC_CHANNEL_8;
  sConfig.Rank = ADC_REGULAR_RANK_1;
  sConfig.SamplingTime = ADC_SAMPLETIME_2CYCLES_5;
  sConfig.SingleDiff = ADC_SINGLE_ENDED;
  sConfig.OffsetNumber = ADC_OFFSET_NONE;
  sConfig.Offset = 0;

  if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) {
    Error_Handler();
  }
}
void dmaInit() {

    /* DMA controller clock enable */
    __HAL_RCC_DMAMUX1_CLK_ENABLE();
    __HAL_RCC_DMA1_CLK_ENABLE();

    /* DMA interrupt init */
    /* DMA1_Channel1_IRQn interrupt configuration */
    HAL_NVIC_SetPriority(DMA1_Channel1_IRQn, 0, 0);
    HAL_NVIC_EnableIRQ(DMA1_Channel1_IRQn);
    //HAL_DMA_IRQHandler(&hdma_adc1);

    /* ADC1 Init */
    hdma_adc1.Instance = DMA1_Channel1;
    hdma_adc1.Init.Request = DMA_REQUEST_ADC1;
    hdma_adc1.Init.Direction = DMA_PERIPH_TO_MEMORY;
    hdma_adc1.Init.PeriphInc = DMA_PINC_DISABLE;
    hdma_adc1.Init.MemInc = DMA_MINC_ENABLE;
    hdma_adc1.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;
    hdma_adc1.Init.MemDataAlignment = DMA_PDATAALIGN_HALFWORD;
    hdma_adc1.Init.Mode = DMA_CIRCULAR;
    hdma_adc1.Init.Priority = DMA_PRIORITY_HIGH;
    if (HAL_DMA_Init(&hdma_adc1) != HAL_OK) {
      Error_Handler();
    }
    __HAL_LINKDMA(&hadc1,DMA_Handle,hdma_adc1);
}

void initProcess(void) {
    dmaInit();
    adcInit();
    HAL_ADC_Start_DMA(&hadc1, &buffer, 1);
}

 

1 REPLY 1
mƎALLEm
ST Employee

Dear @fiona_io ,

Please in next time use </> button instead of "Spoiler Tag" button to paste your code.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.