2024-06-12 02:34 AM
ADC1_IN1 |
ADC2_IN3 |
ADC3_IN1 |
As i want to measure few signals simultaneously.
can i configure by this way like ADC1, ADC2, ADC 3
or Separate channels from same ADC1
2024-06-12 02:53 AM
Hello,
Not sure what do you mean by "to measure few signals simultaneously."!
You need to refer to the reference manual RM0440 for that:
From ADC introduction:
The modes are described in the ADC section:
ADC1 and ADC2 can work together in Dual mode in specifically in "Regular simultaneous mode":
See figure 139:
Triple mode is not available on this product.
Hope I answered your question
2024-06-12 03:01 AM
Lets say i want to measure 6 ADC input simultaneously.
Then i have to use 3 channels from ADC1 and rest 3 channels from ADC2.
I am using STM32G474VET3 (G4 series)
2024-06-12 03:14 AM
Again, "6 ADC input simultaneously." is not clear.
The simultaneous mode is described in the RM, you can measure only two channels at time T with two ADCs.
2024-06-12 03:19 AM
SIX (6) ADC input signals to be measured simultaneously.
Like ADC 1 channel input 1 to temperature measurement
Like ADC 1 channel input 2 to current measurement
and so on
2024-06-12 03:22 AM - edited 2024-06-12 04:35 AM
Do you mean in a sequence of 6 channels?
Input 1 then input 2, Input 3 ...until input 6? not sampled at the same time (successively not simultaneously)?
2024-06-12 04:45 AM
This is very simple question
Input 1 then input 2, Input 3 ...until input 6 need to be measured simultaneously.
Does is possible by ADC1 and ADC 2
Input 1 then input 2, Input 3 to ADC1
Input 4 then input 5 , Input 6 to ADC2
i cant elaborate more on this
2024-06-12 05:01 AM - edited 2024-06-12 05:07 AM
"Does is possible by ADC1 and ADC 2
Input 1 then input 2, Input 3 to ADC1
Input 4 then input 5 , Input 6 to ADC2"
This is not a simultaneous conversion. It's a done successively ... and can be done by 2 ADCs in DUAL mode.
I've already shared a figure from the RM that fits your needs ..
And simultaneous conversion is something else, that's why:
"This is very simple question " -> Sorry this is not a simple question .. You need to find the right words to describe what you need ..
2024-06-12 05:54 AM - edited 2024-06-12 05:57 AM
How to do in simultaneous mode then,
I explained these wordings earlier too and never talk about sequential
If need to measure all 6 signals simultaneously
i want to measure 6 ADC input simultaneously.
I can raise my question with another post if not able to get satisfactory answer by STM