ADC, sampled values shows large changes if sampled continuously
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-06-20 04:24 AM
I am using PB0 - ADC2-IN8, as analog input with 10K source impdence. I have configured the pin and sampled continuosly. Values shown shows gradual decrease if delay not added b/w two samples. I am using software control/single conversion method.
below is my code:main(){ GPIO_InitTypeDef GPIO_InitStruct; ADC_CommonInitTypeDef ADC_CommonInitStruct; ADC_InitTypeDef ADC_InitStruct; /* Configure ADC2 for keypad adc, PB0 (IN8) */ /* Enable clock to ADC2 */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC2, ENABLE); /*Enable the AHB1 peripheral clock for portB & configure for ADC */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE); GPIO_InitStruct.GPIO_Pin = GPIO_Pin_0; GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AN; GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOB, &GPIO_InitStruct); /* configure global parameters */ ADC_CommonInitStruct.ADC_Mode = ADC_Mode_Independent; /* ADC1,ADC2,ADC3 operate independently */ ADC_CommonInitStruct.ADC_Prescaler = ADC_Prescaler_Div2; /* ADC freq = 30Mhz */ ADC_CommonInitStruct.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled; /* No DMA access */ ADC_CommonInitStruct.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles; /* time b/w two conversion, not used */ ADC_CommonInit(&ADC_CommonInitStruct);/* ADC2 Init */ ADC_InitStruct.ADC_Resolution = ADC_Resolution_12b; /* 12 bit resolution */ ADC_InitStruct.ADC_ScanConvMode = DISABLE; /* Disable the scan conversion so we do one at a time */ ADC_InitStruct.ADC_ContinuousConvMode = DISABLE; /* Single conversion */ ADC_InitStruct.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;/* No external conversion */ ADC_InitStruct.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T1_CC1; /* Assign value, but not used */ ADC_InitStruct.ADC_DataAlign = ADC_DataAlign_Right; /* data align right */ ADC_InitStruct.ADC_NbrOfConversion = 1; /* Number of channled to scan = 1 */ ADC_Init(ADC2, &ADC_InitStruct); /* Init the ADC */ ADC_RegularChannelConfig(ADC2 , 8 , 1, ADC_SampleTime_15Cycles); /* Enable ADC2 */ ADC_Cmd(ADC2, ENABLE); cnt = 0; while(1) { ADC_SoftwareStartConv(ADC2); while(ADC_GetFlagStatus(ADC2, ADC_FLAG_EOC) == RESET); adc_val = ADC_GetConversionValue(ADC2); my_arr_1[cnt++] = adc_val; configure_tim3_wait(1000); /* Delay added here */ if( cnt == 4800 ) { __NOP(); while(1); } } }Case 1:Without using delay, when I sampled 4800 values, I saw gradual decrease from 4095(full scale) to 4000(approx) at last values.I am writing every 500th values for reference:my_arr_1[0] = 4089my_arr_1[500] = 4029my_arr_1[1000] = 4019my_arr_1[1500] = 4027my_arr_1[2000] = 4013my_arr_1[2500] = 4063my_arr_1[3500] = 3997my_arr_1[4799] = 4021case 2:If delay is added as I marked , then values don't vary like this- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-06-20 04:26 AM
delay added is in microsecond, i.e 1000us
& CPU is running at 120mhz , ADC = 30Mhz- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-06-20 06:20 AM
It sounds the ADC acquisition is disturbing the output of whatever you're measuring. The output then does not have time to settle. Try a longer ADC_SampleTime_<n>Cycles value. Have someone look at the dynamic behaviour of the output you're measuring. Can you look at it with an oscilloscope? Maybe you need to buffer it?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-06-20 07:27 AM
You have to consider the total time needed for conversion including the sampling time. That is why a delay may be required.
In F30x, there is the ''auto-delayed conversion'' feature that provides automatic control. -Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-06-20 07:42 AM
With a 10K input impedance, the ADC channel sample and hold capacitor doesn't have enough time to charge up to the input voltage. You may not see this effect well on an oscilloscope. John F's solution is correct, increase the ADC sampling time from 15 cycles to some larger amount that produces acceptable accuracy, and discard the software delay.
John F's other solution is another correct one. A buffer amplifier will reduce the source impedance to near zero. Cheers, Hal- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-06-20 07:58 AM
I am using STM32F205, I have calculated formula by datasheet & 15 cycles is fine for it. ADC cap will charge in that time. I will also try by 28 cycles or more & will see the results.
But how can adding delay time give right results. ADC will be sampled for same time irrespective of delay introduced.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-06-20 08:56 AM
''I have calculated formula by datasheet & 15 cycles is fine''. Good. I was also concerned if the output of the device you're measuring was capable of driving the ADC input quickly and repeatedly. Sometimes the
dynamic
performance of devices is not obvious. Maybe you have some other problem ...- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-06-20 09:15 AM
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-06-21 02:11 AM
I tried by 28 cycles, but same results were obtained.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-06-21 02:13 AM
I tried by 28 cycles, but same results were obtained.