2020-07-28 5:28 AM
Hello,
Since two year, I am experiencing an issue with the ADC_CHANNEL_12 (pin PC12) of my STM32F767. I suspect it's a hardware issue coming from the MCU.
I use a proper custom PCB circuit, no noise / EMI should be added. Again, the 3 other ADC input pins (PC3, PA0, PA1) are very accurate. Also tested with an oscilloscope, the signals are very clean.
What I've tried:
Maybe some of you came across this issue?
Thanks a lot for your help!
Cheers,
2020-07-28 5:31 AM
void Adc::Init()
{
ADC_ChannelConfTypeDef sConfig;
hadc2.Instance = ADC2;
hadc2.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV8;
hadc2.Init.Resolution = ADC_RESOLUTION_10B; // 10B = PC2 is not offseted anymore
hadc2.Init.ScanConvMode = ENABLE;
hadc2.Init.ContinuousConvMode = ENABLE;
hadc2.Init.DiscontinuousConvMode = DISABLE;
hadc2.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc2.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc2.Init.DataAlign = ADC_DATAALIGN_LEFT;
hadc2.Init.NbrOfConversion = 2;
hadc2.Init.DMAContinuousRequests = ENABLE;
hadc2.Init.EOCSelection = DISABLE;
HAL_ADC_Init(&hadc2);
sConfig.Channel = ADC_CHANNEL_12; // PC2
sConfig.Rank = 1;
sConfig.SamplingTime = ADC_SAMPLETIME_480CYCLES;
sConfig.Offset = 0;
HAL_ADC_ConfigChannel(&hadc2, &sConfig);
sConfig.Channel = ADC_CHANNEL_13; // PC3
sConfig.Rank = 2;
sConfig.SamplingTime = ADC_SAMPLETIME_144CYCLES;
HAL_ADC_ConfigChannel(&hadc2, &sConfig);
if(HAL_ADC_Start_DMA(&hadc2, (uint32_t*)&DMAvalues[0], 2) != HAL_OK) __DEBUG_BKPT();
hadc1.Instance = ADC1;
hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV8;
hadc1.Init.Resolution = ADC_RESOLUTION_12B;
hadc1.Init.ScanConvMode = ENABLE;
hadc1.Init.ContinuousConvMode = ENABLE;
hadc1.Init.DiscontinuousConvMode = DISABLE;
hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc1.Init.DataAlign = ADC_DATAALIGN_LEFT;
hadc1.Init.NbrOfConversion = 2;
hadc1.Init.DMAContinuousRequests = ENABLE;
hadc1.Init.EOCSelection = DISABLE;
HAL_ADC_Init(&hadc1);
sConfig.Channel = ADC_CHANNEL_0; // PA0
sConfig.Rank = 1;
sConfig.SamplingTime = ADC_SAMPLETIME_480CYCLES;
sConfig.Offset = 0;
HAL_ADC_ConfigChannel(&hadc1, &sConfig);
sConfig.Channel = ADC_CHANNEL_1; // PA1
sConfig.Rank = 2;
sConfig.SamplingTime = ADC_SAMPLETIME_480CYCLES;
HAL_ADC_ConfigChannel(&hadc1, &sConfig);
if(HAL_ADC_Start_DMA(&hadc1, (uint32_t*)&DMAvalues[2], 2) != HAL_OK) __DEBUG_BKPT();
/* reduce the ADC noise ? STM32F7 errata sheet */
//SET_BIT(PWR->CR1, PWR_CR1_ADCDC1_Pos);
SET_BIT(SYSCFG->PMC, SYSCFG_PMC_ADC1DC2);
SET_BIT(SYSCFG->PMC, SYSCFG_PMC_ADC2DC2);
}
2020-07-28 7:32 AM
Write a minimal program which does nothing just reads this one ADC channel, to memory, and observe the result with debugger.
JW
2020-07-28 7:52 AM
you could try to change Ranks of ADC_CHANNEL_12 and ADC_CHANNEL_13 to check if anything changes..
Another thing: did you test with HAL_ADCEx_Calibration_Start if this changes anything?
2020-07-29 3:17 AM
Hi, thanks a lot for your help!
2020-07-29 4:15 AM
Does this happen on different layouts? If you didn't test with a totally different layout:
What signal run near to PC12? Maybe there is excessive noise . Or s there perhaps any signal > VDDIO on a TTa pin?
Perhaps try to reproduce on a Nucleo or Disco board.
2020-07-29 4:31 AM
No, indeed the next step is to test it on a new PCB, will do it in the following months!
There is no noisy or high-speed signals next to PC12 ...
Or s there perhaps any signal > VDDIO on a TTa pin?
A TTa pin is a pin that can be declared as an analog input (connected to ADC) ?
If yes, is that possible that having for example a +5V on a TTa pin (even if this pin is not declared as an analog input) can influence the ADC_CHANNEL_12 ?
2020-07-29 1:35 PM
> having for example a +5V on a TTa pin
That's definitively a no-no which may damage the part, not just influence the ADC readings.
Cut the offending signal and retry with the ADC.
JW
2020-07-30 12:58 AM
Thanks for this tip, didn't really aware of that! After double checking my design, no pins of my STM is connected to something more that 3.3V, so I guess that's not the problem.
The next step is to test ADC_CHANNEL_12 on a new design, or a demo board. But the fact that I was able to remove the ADC "random offset" of PC2 by changing ADC_RESOLUTION_12B to ADC_RESOLUTION_10B still seems like a STM32 issue for me :)