cancel
Showing results for 
Search instead for 
Did you mean: 

Activating USART

DKalm.1
Associate II

Hi,

I have a Problem with the NUCLEO-L476RG.

I tried to activate USART2.

Sending a single Char to a Terminal Programm like Putty or HTERM.

I took the guide from the reference Manual on Page 1341.

But it wont work.

#include "stm32l4xx.h"
#include "stm32l4xx_nucleo.h"
 
int main(void)
{
     //MSI CLK setup
     RCC->CR |=RCC_CR_MSIRGSEL;// enable the MSI CLK
     RCC->CR      &= RCC_CR_MSIRANGE_0; 
     // deleting the reset value
     RCC->CR      |= RCC_CR_MSIRANGE_11;
     // setting MSI CLK to 48MHz
     
     // USART Setting
     RCC->AHB2ENR |= RCC_AHB2ENR_GPIOAEN;
     GPIOA->MODER &= ~GPIO_MODER_MODER2_1;
     //alternetive mode for PA2
     GPIOA->AFR[0] |= 0b0111 << GPIO_AFRL_AFSEL2_Pos;
     //alternetive function 7 for PA2
     RCC->APB1ENR1 |= RCC_APB1ENR1_USART2EN;
     //enable clock for Usart2
     
     //Guide on Page 1341
     USART2->CR1 |= USART_CR1_M; 
     // setting the word length
     USART2->BRR = 417; 
     // setting 115200 Baud  
     //=> 48e6/115200=416,666666
     
     // Stop Bit Programming not necessary, 
     //reset value -> 1 Stop Bit
     
 	 // DMA not necessary , or isn't it ?
 	USART2->CR1 |= USART_CR1_UE|USART_CR1_TE; 
 	// USART2  Enable  , Transmitter Enable
 
 	char c = 'C';
 
     for(;;){
                volatile unsigned int i =4800000;
                while(i--);
                while (
                (USART2->ISR & USART_ISR_TXE) == 0);
                  	
                 USART2->TDR=c;
          }
 
}

Have i forgotten something or done anything wrong?

Thanks,

Dominik

​

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

Honestly, if you choose to program at the register level, you really need to learn how to debug at that level also.

If the debugger has a "Peripheral View" use that to descend into the register nodes and check them against expectations set by the Data Sheet and Reference Manual.

Pretty sure you can't arbitrarily change the clock you're currently running from.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User

> Pretty sure you can't arbitrarily change the clock you're currently running from.

Namely you can't switch to high clock without changing FLASH latency (and in some families, maybe not in 'L4, internal LDO regulator setting).

JW