cancel
Showing results for 
Search instead for 
Did you mean: 

Access UART in STM32F303RE Nucleo board

swarnkarankit47
Associate II
Posted on May 02, 2016 at 14:50

Hello,

Please help me to access uart in stm32f303re  Nucleo board and provide me code to do so.

#stm32f303ret6 #nucleo
2 REPLIES 2
Posted on May 02, 2016 at 15:01

Presuming is uses the same USART2 and PA2/PA3 pins like the others, the code will look materially like that for the other STM32 parts.

[DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Discovery/USART%20example%20code%20for%20Nucleo%20F401RE&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F&currentviews=2302]https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2FSTM32Discovery%2FUSART%20example%20code%20for%20Nucleo%20F401RE&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F¤tviews=2302

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Amel NASRI
ST Employee
Posted on May 06, 2016 at 12:24

Hi swarnkar.ankit,

If you need to use Cube with its HAL drivers, I recommend you to start with examples available in STM32Cube_FW_F3_V1.4.0\Projects\STM32F303ZE-Nucleo\Examples\UART to build your own application.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.