cancel
Showing results for 
Search instead for 
Did you mean: 

About the DS11532

Issamos
Lead III

Hello ST Community team,

On the DS11532: 

  • The title of the Figure 20 should be changed to avoid any confusion between figure 20 and figure 21.
  • Also, the note under figure1 is not really clear since the STM32F767 TFBGA216 for example is not compatible pin to pin with the STM32F469 TFBGA216. So, I think the note should be clearer. It can even point to the application note AN4660 for details.

Could you please have a look.

Best Regards.

II

1 ACCEPTED SOLUTION

Accepted Solutions
Imen.D
ST Employee

Hi @Issamos ,

There is no duplication for Figure 20 and 21 as: Figure 20. is for STM32F76xxx TFBGA216 and Figure 21. for STM32F769xx TFBGA216 with DSI.

I escalated your issue regarding the text below the figure1 to clarify this (internal ticket number: 221536).

Thank you for your contributions.

(PS: Internal ticket number 221536 is not accessible or usable by customers).

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

View solution in original post

3 REPLIES 3
Imen.D
ST Employee

Hello @Issamos ,

Thank you for having reported this.
I will check this and come-back to you soon with updates.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Imen.D
ST Employee

Hi @Issamos ,

There is no duplication for Figure 20 and 21 as: Figure 20. is for STM32F76xxx TFBGA216 and Figure 21. for STM32F769xx TFBGA216 with DSI.

I escalated your issue regarding the text below the figure1 to clarify this (internal ticket number: 221536).

Thank you for your contributions.

(PS: Internal ticket number 221536 is not accessible or usable by customers).

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

Hi @Issamos ,
After deep check, we have concluded that the STM32F76x and STM32F4xx devices are indeed pin-to-pin compatible when not considering packages that include the DSI peripheral.

So, the following sentence in DS11532 under Figure 1 (page 19) :

"The STM32F76x LQFP144, LQFP176, LQFP208, TFBGA216, UFBGA176 packages are fully pin to pin compatible with STM32F4xx devices."

will be changed to:
“The STM32F76x and STM32F4xx devices are indeed pin-to-pin compatible when not considering packages that include the DSI peripheral.”

For further details, I recommend consulting AN4660, section 1.1.4 “TFBGA216 package,” which provides a through explanation of this compatibility.

Thank you for your contribution.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen