cancel
Showing results for 
Search instead for 
Did you mean: 

What is the state of the GPIO of the STM32F767ZIT6 during reset and after reset before configuration?

MAndr.4
Associate

The notes in the STM32F76xxx data sheet DS11532 Rev 7 give 2 different answers to this question. See attached. I'm guessing the default state of the unconfigured GPIO is "Floating Input."

1 REPLY 1

There are a couple of exceptions, as noted by the register initialization values,but yes mostly input/floating. ie transistors both off, pull up/down resistors not connected.

Analogue Input would be where the digital schmitt trigger on the input is disabled, so nothing internally is going to react to a perceived potential change on the pin itself

Tips, buy me a coffee, or three.. PayPal Venmo Up vote any posts that you find helpful, it shows what's working..