cancel
Showing results for 
Search instead for 
Did you mean: 

about stm32G070 temperature sensor

LOMO
Associate III

cannot find TS_CAL2 in datasheet0693W00000WJUv8QAH.png

1 ACCEPTED SOLUTION

Accepted Solutions

Well, the internal temperature sensor is based on a pn junction through which a constant current flows and whose temperature coefficient of approx. -2mV/K is used to determine the current chip temperature. However, even after calibration, its accuracy cannot be compared with that of an external temperature sensor.

Depending on your requirements for "precise temperature measurement", an external sensor may be the only option, or alternatively the STM32G071, whose value is measured for TS_CAL2.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

5 REPLIES 5
Peter BENSCH
ST Employee

Welcome, @LOMO​, to the community!

This is a known issue of RM0454, which is already being worked on to fix.

Cause: the STM32G070 belongs to the so-called Value Line, which are produced in a cost- and thus price-optimised way, which does not allow the measurement of TS_CAL2. The next revision of RM0454 will contain a corresponding correction in section 14.9.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
LOMO
Associate III

Is there any oteher solution to measure precise temperature of stmG070 device,as TS_CAL2 is invalid.0693W00000WJXdCQAX.jpg

Is there any oteher solution to measure precise temperature of stmG070 device,as TS_CAL2 is invalid.0693W00000WJXdCQAX.jpg

Well, the internal temperature sensor is based on a pn junction through which a constant current flows and whose temperature coefficient of approx. -2mV/K is used to determine the current chip temperature. However, even after calibration, its accuracy cannot be compared with that of an external temperature sensor.

Depending on your requirements for "precise temperature measurement", an external sensor may be the only option, or alternatively the STM32G071, whose value is measured for TS_CAL2.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

OK,Thanks.