2014-04-16 01:11 AM
Hello
Thehttp://www.st.com/web/catalog/tools/FM116/SC959/SS1532/PF259090
has a few Free I/O Pins. Is there a list of alternate functions of those pins? It's not mentioned in the corresponding documentation DocID025175 Rev 1 I'm trying to evaluate whether the few I/O Pins are suitable for me or not. Regards Chriostoph2014-04-21 12:13 PM
Are you sure it is correctly orientated? ie Rotated with respect to Pin 1?
Attach a picture (use macro setting, have it focused)2014-04-21 12:23 PM
2014-04-21 12:35 PM
Yes, so you've got the orientation wrong
2014-04-21 12:58 PM
Thank you..It worked .... I was confused by the logo orientation on STM32CubeMx...I didn't see the circle markation... Thank you again
2014-04-22 04:45 AM
2014-04-22 08:18 PM
2014-04-30 03:40 PM
OOPS, Christof,
I think you may have missed four pins. PA7, PB2, PC14, & PC15.2014-04-30 04:37 PM
PC14/PC15 are typically used for the 32.768 KHz crystal, they are in the low/backup power domain, and can only sink 3mA. Use them as GPIO with caution.
2014-04-30 06:30 PM
Thank you very much for that advice. I was not aware of that.