cancel
Showing results for 
Search instead for 
Did you mean: 

32F429I discovery power off LCD

mats23
Associate II
Posted on May 30, 2014 at 14:14

Hi,

I have a 32F429I discovery board and I am trying to put it into sleep mode using a call to HAL_PWR_EnterSTOPMode . I believe that this works, but I would also like to turn off the display when doing this.

Is there an easy way to do this?

/Mats
2 REPLIES 2
Posted on May 30, 2014 at 15:36

I'm not sure there is, I remember having a discussion about the back light, pretty sure it can't be turned off. Check the schematic for pin/control options.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
mats23
Associate II
Posted on June 02, 2014 at 11:43

I believe that you are right, I cannot find anything in the schematics indicating a control of the back light.

Thanks!