cancel
Showing results for 
Search instead for 
Did you mean: 

24-RGB LTDC ESD Protection

nman
Associate

Hi. When utilizing a 24-RGB interface, should each individual signal line be equipped with ESD protection? This would demand a small army of TVS diodes/arrays, which is fine, just want to make sure that this is an industry-standard approach.

Thanks.

1 REPLY 1
STOne-32
ST Employee

Dear @nman ,

Welcome in STCommunity .  Indeed this will depend on your application : industrial /consumer products and the level of ESD protection to reach on top of our GPIOs . You can see our reference demonstration boards and connected LCDs :

https://www.st.com/resource/en/application_note/an4861-introduction-to-lcdtft-display-controller-ltdc-on-stm32-mcus-stmicroelectronics.pdf

Have a great day,

STOne-32