2 bit RTC->DR problem for STM32F767 (corrected title)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-06-23 4:17 AM
I am using STM32F767, unfortunately I have a problem with the DR register area in the RTC. Exactly the problem is with the 10th and 17th bits of this register. Setting "1" means that I am not able to change these bits to "0". Only resetting the BDCR helps. Interesting fact: In the case of automatic date change (i.e. from July 31 to August 1) bit 10 in the DT register is automatically reset. Where could the problem be?
- Labels:
-
RTC
-
STM32F7 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-06-28 10:51 AM
Thanks for the answer and suggestions.
Registers after reset,
RTC-> TR = 0x52
RTC-> DR = 0x2101
RTC-> CR = 0
RTC-> ISR = 0x27
RTC-> PRER = 0x7f00ff
RTC-> WUTR = 0xffff
RTC-> ALRMAR = 0
RTC-> ALRMBR = 0
RTC-> SSR = 0x20
Then I program the time and date:
by setting in advance
RTC-> CAP = 0xCA;
RTC-> CAP = 0x53;
and ISR
Date: 0x224628
Time: 0x193032
Immediately after sending the date and time to the register
RTC-> TR = (uint32_t) tmpTime;
RTC-> DR = (uint32_t) tmpreg;
and
RTC-> ISR & = (uint32_t) ~ RTC_ISR_INIT;
The registers are as follows:
RTC-> TR = 0x193032
RTC-> DR = 0x224628
RTC-> CR = 0
RTC-> ISR = 0x37
RTC-> PRER = 0x7f00ff
RTC-> WUTR = 0xffff
RTC-> ALRMAR = 0
RTC-> ALRMBR = 0
RTC-> SSR = 0
From now on, I will not present the bits I mentioned earlier (the rest can be changed)
Registers after trying to set the time to August 1, 2022:
(tmpreg = 0x222801
tmpTime = 0x194041)
RTC-> TR = 0x194041
RTC-> DR = 0x222c01
RTC-> CR = 0
RTC-> ISR = 0x37
RTC-> PRER = 0x7f00ff
RTC-> WUTR = 0xffff
RTC-> ALRMAR = 0
RTC-> ALRMBR = 0
RTC-> SSR = 0xfd
Vbat is stable
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-06-28 12:01 PM
I see.
This all looks OK (except for the result).
Does the unexpected value in DR persist even after some time, when TR changes naturally from running RTC?
Can you please set RTC->CR.BYPSHAD=1, and then try to do the same?
How is the APB1 clock set? And how is RTC clocked?
JW
PS. RTC-> CAP? Do you mean RTC->WPR?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-06-29 4:32 AM
As I wrote earlier, the DR value changes correctly by itself. The problem only affects the update and only 2 bits in the DR register. I don't know what is causing this and I don't understand the mechanism. I also don't know how to do it to set it up correctly. Unfortunately, as I wrote, from time to time, regardless of me, the time and date will be updated.
With RTC-> CR.BYPSHAD = 1 set, it behaves identically. The difference is that in debugging I can change the date in the DR register by "clicking the mouse" (unfortunately when I change bits -10 and 17 in RTC-> DR to "1", I am not able to change them back to 0). The RTC clock is clocked from a LSE 32768Hz oscillator.
APB1 - peripheral clocks: 54MHz; APB1 Timer clocks: 108MHz.
I did a quick support for Ethernet only, from where I download the time update and only the RTC. The behavior is identical.
RTC-> CAP? Do you mean RTC->WPR?
Yes, I was wrong. Sorry
I will also add that at the end of the function that sets the time and date registers, I put RTC-> WPR = 0xFF;
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-06-29 1:02 PM
Hummm....
I am out of ideas at this point. I also don't have a 'F767 to try. You may want to contact ST directly, through FAE or through the web support form.
JW
PS. @Peter BENSCH , don't you happen to have a 'F767 to try to reproduce this?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-07-01 12:01 AM
Unfortunately not, but I will try to get a board with STM32F767 and follow this up, but I ask for patience.
Regards
/Peter

- « Previous
-
- 1
- 2
- Next »