2025-07-03 7:58 AM
Hello,
We are working on a stm32f429.
The application uses ADC1 to sample data on Channel 0-7.
ADC1 and channels characteristics are:
- Mode: Independant
- Sampling clock: Around 2.8 Mhz
- No DMA access
- Sampling delay: 20 clocks periods (max value)
- Resolution: 12 bits
- No scan mode
- NO continuous conversion
- Single conversion mode
- Channel sampling time is 480 clock cyles (max value)
- Vref+ = Vdda = 3.3V
- VSS = 0V
Each channel is connected to a sensor with a voltage variation of 0-3.30V.
The signal on each channel is a low frequency.
The sampling period for all channel is 1 second.
Channels are sampled alternatively in the following order 0,1,2..7.
This works pretty well, with a very good precision for our application.
Now the specific issue we have is:
Each channel has it owns conditionning chain independant from the others.
We have ruled out the conditionning chain as the source of the problem.
Because the input signal on Channel N+1 is stable when the voltage measured by the ADC is reduced by 0.3V.
Our Hypothesis:
We know that during each sampling phase, Channel N for example, the ADC
capacitors are charged up with the channel voltage: 3.3V for example.
At the end of the conversion, the capacitors are not discharged.
At the next sampling phase, Channel N+1, the new channel voltage is 1 V for example.
When the ADC sampling switch is closed, a charge transfer begins between the ADC
capacitors at 3.3V (Channel N value) and channel N+1 at 1V until equilibrium is reached or the adc
sampling time is reached.
If the sampling time is reached before the equilibrium, the ADC caps will holds
a voltage value different from the real channel value => which will produce an erroneous value.
To correct the problem, we have tested two solutions:
Solution 1: Using a dummy channel
We've set up an unused ADC channel tied to GND: let's say a dummy channel.
Then we sample this dummy channel before sampling any real channel.
This approach produce valid data on each channel and solves the problem.
Note: When the Dummy channel is tied to 3.3V, the problem remains.
Solution 2: Reducing the ADC frequency
By reducing the ADC frequency from 2.8 Mhz to 1.4 Mhz, The problem is solved.
We don't have a deep understanding on the problem at stake here. we have two question:
1 - Has anyone ever had this problem ?
2 - Is our hypothesis pointing to the problem root cause ?
2025-07-09 3:21 AM
Have you observed the ADC inputs with a scope?
2025-07-09 7:34 AM
Prepare a minimal but complete compilable code exhibiting the problem, and post.
JW