2021-02-08 11:41 PM
Hi,
I am working on a project using STM32F7. So far I have touchgfx working with external QSPI for storing image resources. Everything is working good and expected so far.
Now I would like to add audio functionality. The aim is to play WAV files when a touchgfx button is present. I am planning to use x-cube audio framework for the audio part.
What I am not clear about are
thank you for the help
2021-02-18 04:42 AM
Hi,
Have you been able to find a solution to this ? If not then this will put the post back up for more visibility 😅.
Concerning the qspi memory, unless I am mistaken you cant divide it into two sections, one memory mapped the other not.
/Romain
2021-02-18 08:29 AM
Hi Romain,
Unfortunately no. I have gone through touchgfx documentation as well and they dont have any information on this. I am not surprised, given touchgfx does not have any audio support. What I am surprised is that no one has run into this use case? Seems like a fairly common use case.
As a last resort, I was thinking of adding a SD card interface and use it for audio storage (and qspi for touchgfx storage). Shold work, its just seems very wasteful.
2021-02-18 08:40 AM
Write the DISKIO layer for FATFS to read from addressable memory space, like it would for a RAMDRIVE. Have FATFS do READ ONLY
Build a disk image with something like WINIMAGE, and write that binary image deeper into QSPI, ie at 0x90100000 (or wherever) outside of the scope of data you told the linker you had in the linker script / scatter file.