2023-10-12 04:02 PM
Dear,
I am currently in the process of designing a custom PCB with your STM32WLE5CCU6 chip (QFN Package). Consequently, I have a few questions:
Given that the PCB will be exclusively sold in Europe and that I need to optimize power consumption, should my design align with the schematic provided in the attachment (MB1720-HighBand_LowPower-A01_Schematic_Internal)? I assume that due to the geographic location, I should use the High Band version. Please confirm this for me.
Can we purchase your PCB with this chip (MB1720)?
Can I power all peripherals with LiSOCl2 batteries recommended for LoRa applications? The rated voltage of these batteries is 3.6 V.
Thank you in advance!
Sincerely,
Zelimir Trisic