2024-07-29 09:54 AM
Hi all,
Could anyone advise the current status of EPR support on the UCPD software? Thanks.
Best Regards
EY
2024-08-05 12:36 AM
Hello Ey,
The STM32G071B-DISCO doesn't have the necessary hardware equipment to support EPR.
Best Regards,
Lucas
2024-08-05 08:49 AM
Hello,
By "doesn't have the necessary hardware equipment" I mean that STM32G071RB-DISCO can support up to 26V. Beyond this value you could damage the device.
Best Regards
2024-08-05 11:47 AM
Dear Lucas,
Many thanks for following up my query. I was aware of the 26V limit but still would like to know whether EPR voltages below 26V would be supported (in my case it’s 24V with AVS). If not could I do such PD3.1 sniffing with ST TCPP evaluation kits?
Thanks again for your help.
Best Regards
Edwin
2024-08-05 11:55 PM
Hello Ey,
Unfortunately EPR voltages below 26V are not supported either since software don't handle it. To detect EPR voltages, STM32G071RB-DISCO must ask for EPR source capabilities which it doesn't. Thus, you won't be able to detect EPR voltages.
Br,
Lucas