Skip to main content
Associate II
July 15, 2024
Question

Couldn't Find Mac_802_15_4_Sniffer.bin file

  • July 15, 2024
  • 3 replies
  • 1233 views

Hi Community,

I’m trying to use the CubeMonitor-RF sniffing tool to monitor packets between my two NUCLEO-WB55 boards. I have followed all the instructions indicated by UM2288 and the ST Wiki. However, I am confused about the firmware upgrade for the M4 core using the Mac_802_15_4_Sniffer.bin file. I couldn’t find any file named Mac_802_15_4_Sniffer.bin in the en.stm32cubewb-v1-20-0 folder.

Could anyone guide me on where to find this file or provide any additional steps I might have missed?

Thank you!

This topic has been closed for replies.

3 replies

STTwo-32
ST Technical Moderator
July 15, 2024

Hello @iFoX 

For the 802.15.4 sniffer:

The wireless stack is in the \Projects\STM32WB_Copro_Wireless_Binaries\STM32WB5x\stm32wb5x_Mac_802_1 5_4_fw.bin folder. The firmware binaries are Mac_802_15_4_Sniffer_Dongle.bin and Mac_802_15_4_Sniffer_Nucleo.bin. The location changes with the operating system:

a) For Windows, the firmware is in the \STMicroelectronics\STM32CubeMonitor-RF\sniffer folder ,which means C:\Users\Public\Documents\STMicroelectronics\ STM32CubeMonitor-RF\firmwares.

b) For Linux, the firmware is in the /STMicroelectronics/STM32CubeMonitor-RF/sniffer folder.

c) For macOS®, the firmware is inside the document folder provided in the setup package: \Users\Public\Documents\STMicroelectronics\ STM32CubeMonitor-RF\firmwares\Mac_802_15_4_Sniffer.bin

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
iFoXAuthor
Associate II
July 16, 2024

Hi @STTwo-32

 

Yes, I did locate the folder name Sniffer in the C:\Program Files\STMicroelectronics\STM32CubeMonitor-RF\sniffer location, but it consisted of only 2 files named stm32cubeMonRf_sniffer.bat and stm32cubeMonRf_sniffer.py and I couldn't find any other folders or files beside these 2.

 

Thank you for your response.

STTwo-32
ST Technical Moderator
July 24, 2024

I think you have to download the last version of the STM32CubeMonitor-RF.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.