cancel
Showing results for 
Search instead for 
Did you mean: 

I want to upload vdo or audio file to stm32h750b-dk, what should I do?

wsuwa.1
Associate III
 
4 REPLIES 4

Push in via an External Loader, pull via Ethernet, or USB Flash Drive (MSC Host)

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
wsuwa.1
Associate III

Do you have a sample?

Not something I'm working on. Perhaps look if there is an example MSC Device using the eMMC directly?​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
FBL
ST Employee

Hello @wsuwa.1​, 

For audio file, you can get inspired with the example provided for STM32H747I-DISCO as referenced here.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.