cancel
Showing results for 
Search instead for 
Did you mean: 

How to run the STL flash test for the complete flash area even the unused portion?

FURIOUS
Associate

Hello everyone, the STL_programmer currently calculates the CRC only for the in-use memory or up to the binary file size. Is there a way to fill the remaining flash memory with zeros and calculate the CRC for the entire flash area, eliminating the need to constantly update the section value based on the binary size?"

Basically how i can run the STL flash test for the complete flash area even the unused portion, Anyone suggest some way please.

1 REPLY 1
Amel NASRI
ST Employee

Hi @FURIOUS ,

I'm moving this post from the original discussion Solved: Running into a strange problem . We're working on ... - STMicroelectronics Community.

Could you please provide some more details about your current request & the context? 

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.