2021-12-14 02:29 AM
Hi,
as explained into the title, i am developing a firmware on this board which is stable. i have bought a new set of board and after flashed, the firmware becames unstable :unamused_face:
Searching a reason why i have seen that the MCU revision is not the same: Y with my first board set on which the firmware is stable, X with the second set giving unstability. Please what is the problem ? what i need to adapt ?
2021-12-15 11:47 AM
Hi Cedric,
Indeed i observe that the plots are very similar. I do not use SDK, i use cube mx to generate configuration i need and the other part is my own code using some function from HAL library.
2021-12-16 12:55 AM
Hello @coren.1 ,
So the last thing I can suggest you is to use the SDK with your two boards version X and Y and check that you have the same behavior.
Best Regards
Cedric