2023-09-19 09:59 PM
we have a ather electrinc schooter ,they have used the 48 volt motor .motor image is attached .i am confusing that for this motor which board we can use for no load run ?
Solved! Go to Solution.
2023-09-20 05:39 AM
Hello @Ranjeet Singh
I suggest the St Mc Suite tool, which lists you the Motor Control compatible boards with the details, Here is the link : https://www.st.com/st-mc-suite/home/
- Click on - Start -> Engine Control Solution
- select the motor type (BLDC)
- select the algorithm
- then choose your board in Power Board
The STEVAL-CTM009V1 board can meet your expectations.
Regards
2023-09-20 05:39 AM
Hello @Ranjeet Singh
I suggest the St Mc Suite tool, which lists you the Motor Control compatible boards with the details, Here is the link : https://www.st.com/st-mc-suite/home/
- Click on - Start -> Engine Control Solution
- select the motor type (BLDC)
- select the algorithm
- then choose your board in Power Board
The STEVAL-CTM009V1 board can meet your expectations.
Regards
2023-09-21 12:04 AM - edited 2023-09-21 12:11 AM
hi @Zied b.
at 48 volt using STEVAL-CTM009V1 board what maximum current we can draw from this board ?
i think 104 A . am i right ?
2023-09-22 12:56 AM
Hello @Ranjeet Singh
For the voltage you are looking for, you have EvalStDrive101
2023-09-22 02:25 AM
thank you for your support @Zied b.