cancel
Showing results for 
Search instead for 
Did you mean: 

which board is suitable for this motor "mahle 48 volt 3.3KW motor"

Ranjeet Singh
Senior

we have a ather  electrinc schooter ,they have used the 48 volt motor .motor image is attached .i am confusing that for this motor which board we can use for no load run ?IMG20230727115945.jpgIMG20230727115940.jpg

1 ACCEPTED SOLUTION

Accepted Solutions
Zied b.
ST Employee


Hello @Ranjeet Singh 
I suggest the St Mc Suite tool, which lists you the Motor Control compatible boards with the details, Here is the link : 
https://www.st.com/st-mc-suite/home/

- Click on - Start -> Engine Control Solution
- select the motor type (BLDC)
- select the algorithm
- then choose your board in Power Board

The STEVAL-CTM009V1 board can meet your expectations.

Regards

If you agree with my answer, please accept it by clicking on "Accept as solution".

View solution in original post

4 REPLIES 4
Zied b.
ST Employee


Hello @Ranjeet Singh 
I suggest the St Mc Suite tool, which lists you the Motor Control compatible boards with the details, Here is the link : 
https://www.st.com/st-mc-suite/home/

- Click on - Start -> Engine Control Solution
- select the motor type (BLDC)
- select the algorithm
- then choose your board in Power Board

The STEVAL-CTM009V1 board can meet your expectations.

Regards

If you agree with my answer, please accept it by clicking on "Accept as solution".

hi @Zied b.  

at 48 volt using  STEVAL-CTM009V1  board what maximum current we can draw from this  board ?

i think 104 A . am i right ?

Hello @Ranjeet Singh 
For the voltage you are looking for, you have 
EvalStDrive101 

Rated Voltage: [6 - 75] V
Rated Current: 20 A
And STEVAL-CTM009V1
Rated Voltage: [5 - 48] V
Rated Current: 200 A
Both will be supported by MCSDK 6.2 which will be released very soon
If you agree with my answer, please accept it by clicking on "Accept as solution".
Ranjeet Singh
Senior

thank you for your support @Zied b.