cancel
Showing results for 
Search instead for 
Did you mean: 

Where to find STM32F401RE .ioc file compatible with X-CUBE-SPN15?

GFrid.2
Associate II

Hello,

I purchased X-NUCLEO-IHM15A1 DC Brush motor controller, which is supported by BSP X-CUBE-SPN15. Documentation specifies three supported Nucleo-64 boards; I purchased NUCLEO-STM32F401RE.

How to find the F401RE .ioc file to enable resources needed by IHM15A1?

Thank you.

2 REPLIES 2
GFrid.2
Associate II

Apparently the SPN15 software was developed before MX .ioc files where created? Thus no .ioc file?

IHM15A1 mostly works, but still have not determined why Motor B will not run backward with the demo software in DUAL mode. Have replaced both the F401RE MCU and the IHM15A1Motor Driver board. Have also swapped the motors between Channel A & Channel B. The IHM15A!/SPN15 software does not drive Motor B during demo steps 1-4 with the hardware jumper set to DUAL. It all works fine in PARALLEL,

It seems likely that there may be a defect with the particular IHM15A1 expansion boards that I purchased, because it looks like the SPN15 software works just fine.

Mat1
Associate III

An *.ioc file for the X-NUCLEO-IHM15A1 would be very helpful.

Now I have to transfer the old SPN15 world to the new *.ioc world. I will use the X-NUCLEO-IHM15A1 together with the NUCLEO-F091RC.