2023-07-21 9:05 PM
I am running the motor control workbench B-G431B-ESC1 board. The systick fires at every 2K frequency as per the user manual and the waveform matches when i toggle, but the problem is sometimes it misses as shown
I want to debug and find out why it misses those timings in between. Please suggest how do i find out? I am also running CAN in parallel at 500KBPS.
Solved! Go to Solution.
2023-07-26 10:11 PM
I have tried this once but seem to be complete misbehavior, i will try again.
2023-07-26 11:58 PM
2023-07-27 7:52 AM
The problem is it is motor control application so i use all the PWM channels, hence i cannot use the method you suggested for driving the GPIO's.
2023-09-24 10:18 AM
I modified the algorithm of CAN and behavior is ok now, i mean i transmit 3 messages at one time, after 1 sec another 3 messages with total of 12 messages
1st sec -> 3messages
2nd sec -> 3 messages
3rd sec -> 3 messages
4th sec -> 3 messages
repeat like this.