2023-06-07 02:10 AM
I have designed a custom board based on STSPIN32G4 schematic but with an automotive mosfet (iaua200n04s5n010auma1).
Everything works except that the controller enters an IDLE STATE and STOP STATE every time I tried to run the motor.
Does this have to do with the internal Mosfet gate driver?
Thanks, and best regards,
Mit freundlichen Grüßen - with kind regards
2023-06-07 02:40 AM
The controller now works normally if i remove the gate resistor of the mosfets. But i need to know if the controller can drive this mosfets and what is the right gate resistor value?
2023-06-07 03:33 AM
I have changed the value of the gate resistors and the controller doesn't work. It goes to a stop state and an idle state.