cancel
Showing results for 
Search instead for 
Did you mean: 

STSPIN Studio --- Stepper Motor 24BK20-30 --- NucleoF401RE

SWenn.1
Senior III

I have the above subject powered with 24V, 3A power supply.  The motor is not loaded.  I keep having issues trying to write to the device.  How do I get this warning to not appear and why is it appearing?

My second question is when I do BLDC stuff with MC WorkBench it generates an STM32CubeIDE project but I see nowhere within STSPIN to have this done.....How do I transition a working Stepper solution to an STM32CubeIDE project?

SWenn1_0-1713644503231.png

 

3 REPLIES 3
Cristiana SCARAMEL
ST Employee

Hello @SWenn.1 ,

the motor must not be in motion to write the parameters.

The STSPIN Studio is an evaluation software, it does not output a project for STM32.

I hope this post can help you; if so, consider to mark it as best answer by clicking the label "Select as Best".

If you feel a post has answered your question, please click "Accept as Solution"

Hello Cristiana.

Is there a library for powerSTEP01 that can be incorporated into an STM32CubeIDE projects?

If so please point me to the URL.

Steve

Hello @SWenn.1,

unfortunately, there are no library for powerSTEP01 available.

If you feel a post has answered your question, please click "Accept as Solution"