2019-08-15 3:36 AM
Hi
any one can help to me how can start with stm32 with ac induction motor with library st
need some example is possible use motor workbench v5 for setup induction?
Solved! Go to Solution.
2021-06-28 5:47 AM
Dear @omid hamdi
There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.
Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .
Best regards
2021-06-22 1:13 AM
The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
2021-06-28 5:47 AM
Dear @omid hamdi
There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.
Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .
Best regards
2021-07-09 9:25 AM
thanks for help resolved