2020-03-02 2:32 PM
Is it possible to run two or more channels on timer with DMA PWM mode?
This code starts only first Channel.
uint32_t PrawoPWM = 100;
uint32_t LewoPWM = 100;
HAL_TIM_PWM_Start_DMA(&htim4, TIM_CHANNEL_1 , &PrawoPWM, 1);
HAL_TIM_PWM_Start_DMA(&htim4, TIM_CHANNEL_2 , &LewoPWM, 1);
How can I start two channels?
2020-11-02 12:08 AM
Dear @JSzem.1
As you do not answer, I guess you don't have to solve this problem anymore, therefore I consider this thread closed.
If not, feel free to reopen it by posting a new answer.
Best regards
Laurent Ca...