2024-09-14 12:23 AM
Hi,
I have a custom motor control board with STM32F302R8T6 as controller and L9907 as the driver. Could you suggest any example codes I can use for the integration? I could not find anything available in Motor control work bench and AutoDevKit Studio.
Help much appreciated
Best Regardsm
Bala
2024-09-14 03:36 AM
Welcome @BalaB13, to the community!
I am extremely sorry, but these are two components from different application areas. L9907 is a BLDC driver for automotive applications, STM32F302 is an industrial MCU. As no STM32 has automotive certification to date, there is consequently no support for automotive devices. The same applies vice versa: Autodevkit only recognises automotive devices.
Hope that answers your question?
Regards
/Peter
2024-09-20 11:14 PM
Thanks. Could you let me know where I can get the L9907 driver files?
2024-09-21 05:04 AM
The driver files for both automotive microcontrollers SPC560P and SPC56EL are included e.g. in SPC5-MCTK-01.
Regards
/Peter