cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-SPIN3201 not detecting STLink

JDesi.1
Associate II

I have purchased the STEVAL-SPIN3201 board, but the STM32Programmer does not detect the ST-Link, the LEDs are not getting ON. I also purchased the external ST-LINK V2, with that i tried connecting and erased the memory. The USB driver also having problems. Please support to close the issues and program using internal STLink of the evaluation board.

0693W00000NrDGeQAN.jpg0693W00000NrDGZQA3.jpg

11 REPLIES 11

Use better cables? Especially don't use charging cables.

Avoid Hubs, and Docking Stations

Try different ports, try different PCs

A DELL?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

The ST-LINK shouldn't care if board has a loader, or not.

Whether you have specific code that needs to be loaded is another thing.

Usually perhaps best to save the original content before blowing it away.

You should perhaps contact you local ST office, and find the FAE supporting Motor Control

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Does on board ST link for debugging available in the STSPIN3201 board? I mean can we debug without connecting the external dongle STLink? As per the statement in the user guide.

0693W00000NrDhBQAV.jpg 

The board if you see is completely dead with no led ON.

0693W00000NrDgrQAF.jpg 

0693W00000NrDhpQAF.pngI think the LEDs were all OFF after the below operation. I need to make it up and see the LED's working.

cedric H
ST Employee

Hello @JDesi.1​ ,

If I remember correctly this board needs to be powered to be able to connect ST-Link. Did you try with power supply ?

Regards

Cedric

The power supply is required if i try to run the motor, but as a first step i am checking if i can flash software. So, my understanding is, the flashing can happen if i connect a USB port without power source.

0693W00000NrGvpQAF.pngCould you please confirm if erase operation has any affect on the board. The STLink V2 with external dongle, i am able to connect but not with internal STLink. How to proceed for next steps?

One other question in the user there is mention of the below power supply, but no details are provided.0693W00000NrGwOQAV.jpgI feel lot of documentation is missing, with no mention of the PWM signal test points on the board etc.

It says in includes and ST-LINK

If you connected to J6, then you ERASED the ST-LINK device, and that's why that doesn't work.

The target device would need connections via TP16 and TP17

Here's a schematic

https://www.st.com/content/ccc/resource/technical/layouts_and_diagrams/schematic_pack/group0/66/33/fc/8e/84/ea/42/db/STEVAL-SPIN3201%20schematics/files/steval_spin3201_schematic.pdf/jcr:content/translations/en.steval_spin3201_schematic.pdf

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

OP erased the ST-LINK/V2-1, not the STM32F0 part

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thank you for support, how do I restore back the software. Please help.​