2018-02-21 02:35 PM
Hello,
I'm trying to connect to a steval-spin3201, but having no luck. Both ST Motor Control Workbench and ST-LINK cannot find it. If I look in the Device Manager of my PC, I see the 'STMicroelectronics STLink Virtual COM Port (COM4)', so the PC recognizes it, just that I can't connect.
ST Motor Control Workbench says 'Connection failed! No response, check the communication cable, the power on the board or the baudrate', all of which I've done.
Please advise,
Robert
2021-06-27 06:29 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards