cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL IHM034V2 evaluation board, three phase induction motor is not running, PWN and IPM module is not working

MAhme.5
Associate

Hi,

i'm using the a STEVAL-IHM034V2 board for evaluation (PFC + FOC PMSM).

i am using three phase induction motor

well I am using the Motor Control Workbench 5.4.7, for generating code , Keil uVision5 for burring the code in Controller ,  the code is burned through STLink, its burned

but the motor is not started, even not getting the voltage at the output,

PWM is not working , and Inverter part also not working

motor workbench is connect through serial communication , and opened the monitor window and connected, but still not working

need your support and help to operate this board

Thanks a lot in advance

Thanks and Regards

Mudassar

1 REPLY 1
Laurent Ca...
Lead II

Dear @MAhme.5​ 

Have you looked at https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor ?

Best regards