cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-ESC001V1 Motor Pilot connection

tejas_amp
Senior

I have tried connecting both STLink and UART but Motor Pilot is not getting connected, 

ERROR: No STLink VCP detected

I am using (V1.2.9) and tried using older version but still issue persists. Kindly help.

12 REPLIES 12

Hello,

I think I found the issue, as you are using a non official STLink device, the Discover Board function will not work.

You need to load the GUI you need and then manually connect using the correct COM Port.

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.

Hope this will help,
Gaël A.

which GUI file should i load?

Hello,

i'm updated my sw from sdk 6.2 to 6.3 and now the Motor Pilot application does not work.

If i use the older version with simple USB to UART adapter  it works fine.

Any suggestion? How to change the ST VCP settings to simple UART?

The communication menù still in grey color.

Windows 11, MC-SDK6.3.2, CUBE MX6.13.0, CUBE 17.0

Thanks, regards.

Giovanni