cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-ESC001V1 Firmware

tejas_amp
Senior

The provided example firmware of  STEVAL-ESC001V1 in MCSDK workbench, there is no code in main function while loop. As a beginner, I want to ask; How do we can actually give input and monitor motor performance? Like speed, current etc? Is it possible to provide external throttle signal and then use MCI_ExecSpeedRamp() function?

1 ACCEPTED SOLUTION

Accepted Solutions
GMA
ST Employee

Hello @tejas_amp,

Please refer to provided motor control API description in User Manual documentation available through "Workbench tool">About>Documentations>Documentation>"Components", "Motor Control API" link.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA

View solution in original post

1 REPLY 1
GMA
ST Employee

Hello @tejas_amp,

Please refer to provided motor control API description in User Manual documentation available through "Workbench tool">About>Documentations>Documentation>"Components", "Motor Control API" link.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA