cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-CTMV009V1 3ICS.

tezz
Associate

Hi, st team,

mcsdk: 6.2.1

control board: nucleo-g474re

Bridge: XNUCLEO-IHM09M2

Power Board: STEVAL-CTM009V1

We're going to buy around 10k-25k uc per year.

1. STEVAL-CTM008V1 schematic diagram defines that it is possible to use 3 ICS.

tezz_1-1710157997673.png

 

2. X-NUCLEO-IHM09M2 circuit schematic Fig.1 defines that PhC current can be obtained via MC19(PC0)

tezz_2-1710158039410.png

 

I've assembled STEVAL-CTM008V1 with 3-rd magnetic current sensor.

Could you please advise how can it be achieved?

1. Can I configure 3-ICS reading via workbench?

2. If I clone STEVAL board, is it possible to configure the current sensing to read the 3-rd sensor?

 

tezz_0-1710157831120.png

3. Should I modify firmware sources, generated by workbench?

 

Appreciate in advance,

Taras.

1 ACCEPTED SOLUTION

Accepted Solutions
Gael A
ST Employee

Hello tezz,

Currently only the 2-ICS configuration is supported by the MCSDK (latest 6.2.1). Thus, modifying the STEVAL-CTM009 board description won't help you.
You will have to modify the firmware sources to enable 3-ICS configuration for the STEVAL-CTM009.

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.

Hope this will help,
Gaël A.

View solution in original post

2 REPLIES 2
Gael A
ST Employee

Hello tezz,

Currently only the 2-ICS configuration is supported by the MCSDK (latest 6.2.1). Thus, modifying the STEVAL-CTM009 board description won't help you.
You will have to modify the firmware sources to enable 3-ICS configuration for the STEVAL-CTM009.

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.

Hope this will help,
Gaël A.
tezz
Associate

Appreciate