2024-02-06 2:19 AM
Hi,
mcsdk: 6.2.1
control board: nucleo-g474re
Bridge: XNUCLEO-IHM09M2
Power Board: STEVAL-CTM009V1
Motor: Motenergy ME1304
I prepared motor profile for ME1306 with help of EVSPIN32G4 and used in configuration,described above.
But now I get Startup failure on every start. The shaft does not rotate but trembles only.
Can I get any advice how to debug the issue?
Appreciate in advance.
Solved! Go to Solution.
2024-02-21 1:56 AM
Hey @tasifacij
Here are some screenshots that might help you get a better startup procedure.
please note that speed feedback, startup failure, and over current errors may arise due to hardware issues.
Best Regards!
2024-02-06 2:20 AM
And I can rotate the motor if open loop is enabled.
2024-02-21 12:51 AM
Hi @tasifacij , how did you do the Open loop in ctm009v1? can you provide me some insights on it.
2024-02-21 1:30 AM
MotorWorkbench -> StageConfiguration -> OpenLoop checkbox.
Then Motor pilot allows to select it in control mode.
2024-02-21 1:31 AM
My issue was caused by invalid ICS wiring. I read an inversed signal and PI controllers became crazy of that.
2024-02-21 1:43 AM
@tasifacij , which motor control workbench version are you using?
2024-02-21 1:48 AM
@tasifacij I have the ST mc workbench 5.4.8, i don't find any motor pilot, in which version it is available
2024-02-21 1:56 AM
Hey @tasifacij
Here are some screenshots that might help you get a better startup procedure.
please note that speed feedback, startup failure, and over current errors may arise due to hardware issues.
Best Regards!
2024-02-21 2:02 AM
Hey @SivaVishnu09
Motor pilot is available in V6.0.0 and later.
2024-02-21 9:13 PM
thank you @mimho will try as you have mentioned hope it works