2017-08-09 4:44 AM
Posted on August 09, 2017 at 13:44
Hi. I am using MCWB with FOC 4.3. with STSPIN32F0 eval board. I am trying to switch on the bus voltage sensing. When I set it in the WB, compile and upload, it always randomly pops under or overvoltage error. I can read the voltage, and it is truly under (6v) or over (58v) the treshold (which is wrong, because it should be 24v) , but can not start the motor. (The nominal voltage is 24 V) I can measure the divided bus voltage with its own ADC (but I can not use it separately, since it needs the ADC channels to drive the motor with different setup) . It is not an error of wrong parameters, I checked the Drive and Power stage sections both.
Why is this error occuring to me, and what can I do, to determine the source of it? It seems to me, that the busvoltagesensor class is not working, because it reads the bus voltage, but that voltage is wrong. What can I do about it?
2021-06-27 10:58 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards