2018-05-29 11:47 PM
Hello, I downloaded the latest version of st-motor-control. When I open an example, the software informs me that I am using a newer version and must migrate from 4.3 to 5.0.2. I accept.
Now,
I can open the monitor window and I can control the engine. If I want to modify the configuration and generate it, the software informs me that I can not do it because 'F1 mcus not supported in FW for SDK 5.0'
When I load the example, I have the following information:
App: STMCWB
Time: 05/30/2018 08:38:42Project: NonameFilename: F:\MHK\STM32\STEVAL3201\Noname.logType Time Motor Id Message
UNK 08:06:41 The 'Sensor-less (HFI+Observer)' is not supported in the FW for SDK5.0. All parameters will be disabled.UNK 08:06:41 The 'PFC' is not supported in the FW for SDK5.0. All parameters will be disabled.UNK 08:06:41 The 'LCD' is not supported in the FW for SDK5.0. All parameters will be disabled.UNK 08:06:41 F1 mcus are not supported in the FW for SDK5.0UNK 08:06:41 F2 mcus are not supported in the FW for SDK5.0UNK 08:06:41 STSPIN mcu is not supported in the FW for SDK5.0Where can I find an sDK vesion 4.3 ?
Thank.
Christian
2018-06-11 03:57 AM
Dear Christian,
STSPIN3201 and 3202 are now back in the MCSDK 5.1.1 that is available for download.
Regards
Cedric
2021-06-15 01:28 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards