cancel
Showing results for 
Search instead for 
Did you mean: 

Serial Monitor Software

Roberto Giovinetti
Associate III

Hello everyone

I would like to know if there's a stand alone Windows software for monitoring motors: I generated software using Profiler/WorkBench tools, and with WorkBench I can monitor parameters using Monitor function. So we can check temperature, speed, power and so on. The problem is that I have to run WorkBench and open a project to reach monitor tool via serial port.

Now I've to test software in the field, and I would like to use a software similar to monitor, without passing through WorkBench.

Does anybody know if a software like this exist?

Thank you guys

Roberto

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
trgyada
Associate II

I need a program like you said but :thumbs_down: community is worst. I asked a lot of question but never get correct or satisfactory answer.

The community is often a reflection of its members. Most motor stuff is likely done commercially, by people busy with their own work. If you are an ST customer, the means to access engineering support is via your local sales office, and FAE assigned to your account. They usually also carry a list of consultants/contractors with specific expertise.

For field work, you'd presumably want to instrument your own equipment and software so it can output data/telemetry to a technician with a simple terminal application.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Laurent Ca...
Lead II

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards