cancel
Showing results for 
Search instead for 
Did you mean: 

Sensorless FOC - sudden motor rotation change

RReic.2
Associate II

Hi Community

I'm using the following setup:

  • MC Motor Control Workbench v6.0.0
  • STM32 FW V1.5.0 (HAL)
  • Power + Control Board: B-G431B-ESC1
  • Observer + PLL (Sensorless)
  • Motor 10 pole pair
  • Mech. Speed 200rpm

The motor starts and ramps up to 200rpm.

It can now happen that when there is a load change, the rotor suddenly turns at full speed in the opposite direction. The speed is displayed in the Motor Pilot. In this case, however, the phase current looks distorted.

What can be the cause?

5 REPLIES 5
Javier1
Principal

This looks a lot like the set speed functions expect a signed variable, and youre passing an unsigned variable.

Available for consulting/freelancing , hit me up in https://github.com/javiBajoCero

I just press the button on the board which starts the motor with MC_StartMotor1() and no further action. Then this seems to be a problem in the SDK ?

Maybe , check this out https://wiki.st.com/stm32mcu/wiki/STM32StepByStep:STM32_Advance_MotorControl

Available for consulting/freelancing , hit me up in https://github.com/javiBajoCero

yes..already done

RReic.2
Associate II

...this doesn't happen with "CORDIC"