Second NTC_Handle_t type sensor
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-03-07 7:12 AM
uC = STSPIN32G4
second sensor = PA4 (ADC2_IN17)
I have tried add second NTC sensor and using MC functions.
A have added:
sConfig.Channel = ADC_CHANNEL_17; // BEARING_TEMPERATURE
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SamplingTime = ADC_SAMPLETIME_47CYCLES_5;
sConfig.SingleDiff = ADC_SINGLE_ENDED;
sConfig.OffsetNumber = ADC_OFFSET_NONE;
sConfig.Offset = 0;
if (HAL_ADC_ConfigChannel(&hadc2, &sConfig) != HAL_OK)
{
Error_Handler();
}
to MX_ADC2_Init.
I defined :
NTC_Handle_t Temp2Sensor_M1 =
{
.bSensorType = REAL_SENSOR,
.TempRegConv =
{
.regADC = ADC2,
.channel = MC_ADC_CHANNEL_17,
.samplingTime = M1_TEMP_SAMPLING_TIME,
},
.hLowPassFilterBW = M1_TEMP_SW_FILTER_BW_FACTOR,
.hOverTempThreshold = (uint16_t)(OV_TEMPERATURE_THRESHOLD_d),
.hOverTempDeactThreshold = (uint16_t)(OV_TEMPERATURE_THRESHOLD_d - OV_TEMPERATURE_HYSTERESIS_d),
.hSensitivity = (uint16_t)(ADC_REFERENCE_VOLTAGE/dV_dT),
.wV0 = (uint16_t)(V0_V *65536/ ADC_REFERENCE_VOLTAGE),
.hT0 = T0_C,
};
and in main :
NTC_Init(&Temp2Sensor_M1);
Nothing happens... Do You know what I can do next?
Even is it posiible to use diffrerent /anotherADC to RCM_RegisterRegConv() function?
Kind regards
�?ukasz �?ęcki
- Labels:
-
ADC
-
STM32 Motor Control
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-11-15 6:18 AM
Hello,
Firstly, we would like to sincerely apologize for the delay in replying to your post.
If your point is still pertinent, please consider using MCSDK6.2 WorkBench, you will be able to directly edit a board description .json file (starting from an existing one using STMC Board Manager) in order to add your new temperature measurement input as below:
"TEMPERATURE_NTC": [
{
"name": "PC4",
"help": "",
"cost": 0
},
{
"name": "PA4",
"help": "",
"cost": 0
}
Starting a new project with this modified board description, motor control workbench will give you the input choice and will generate the project accordingly.
Best regards.
GMA