2019-10-23 07:24 AM
Hello everybody,
I want to test a BLDC-Motor with the STEVAL-SPIN3202 board and the Motor Control workbench software.
If I start the motor, I always get the message "start up failure" in the monitor of the Motor Control software and the motor doesn't rotate?
Can anybody help me with the settings for a BLDC-Motor in sensorless mode?
2019-10-24 12:51 PM
Hi, Google: "STM PMSM FOC SDK FAQ"
2021-06-21 11:13 PM
The question has been set only to the "STM32 Motor Control" topic (the question is only about the STM32 MC SDK).
Best regards