cancel
Showing results for 
Search instead for 
Did you mean: 

Power Measurement classes

freppa
Associate II
Posted on April 17, 2018 at 17:25

What are the use of the Power Measurement classes in the ST MC FOC lib v4.3?

From the confidential distribution the following classes are part of MC Library module:

MotorPowerMeasurementClass

PQD_MotorPowerMeasurementClass

There is no info on this in UM1053. 

#power-measurement
1 REPLY 1
Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards