2018-04-09 4:26 AM
Does the ST MC FOC lib send an asynchronous message over UART in the event of a fault?
Typically the scenario is that the MCU running the ST MC FOC lib v4.3 detects a fault condition such as over voltage, will it notify the the master (typically PC or other MCU) by sending a message over UART?
Or, do you have to poll the status from master by sending ST Motor Control Protocol message?
#fault-handling #communication2021-06-27 9:08 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards