2020-03-17 12:45 PM
Moved to correct forum, please delete.
I purchased two different ST controller boards:
I also have two motors:
I've tried to profile the motors using the ST Motor Profiler but it always errors with "Profiling takes too much time" at 94% of Electrical parameter detection. The exact same thing happens with both controller boards and both motors. I've tried different combinations of voltage, current and max speed. The motors have 4 pole pairs.
I also tried gathering the information from the datasheet (https://hzmgdj.en.alibaba.com/product/60120702270-200533488/SERVO_MOTOR_OF_80ST_M04025.html) and run the motor in Workbench but I cannot get the motors to run smoothly. They just rapidly move back and forth.
Any help would be greatly appreciated.
2021-06-21 10:45 PM
The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards