2018-05-21 07:58 AM
My end aim is to use #Motor #profiler to workout my motor parameters. I have #nucleo-F302R8 and #X-nucleo-IHM08M1 boards.
I selected these two in Profiler, Connected My motor and Hall devices, Entered 4 Pole pairs and max speed as 4000RPM. Max current as 20A (Motor rated for 30A). Connected Power suppy of 12V/40A . Connected and started Profiling.
Motor moved approx a revolution and stopped. And the after a few minutes and fails. Shows Resistance, Inductance, Supply voltage and current.
What is I am missing ??
Regards
Vimal Amin
2021-06-27 09:57 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards