2022-09-11 11:23 PM
Hi,
I am using motor profiler 5.4.8 with F302R8 and IHM08M1 to get the motor profile of my BLDC motor.
I have a query. Let say the maximum speed i get from the motor profiler is 30krpm. Can i change the maximum speed in motor control workbench (e.g. from 30krpm to 40krpm) and adjust the motor speed up to 40krpm in workbench?
Thanks,
Kim
2022-10-12 09:07 AM
Hello,
Have you set 40krpm on "Max Speed" profiler interface before profiling the motor?
If yes, and if profiler provides a lower max speed than expected, may be that electrical parameters, as Vbus value e.g., have be increased...
On the other hand, yes, you can change the "Max. Application speed" clicking motor "M" on workbench interface.
Best regards.
GMA