cancel
Showing results for 
Search instead for 
Did you mean: 

Motor Control Workbench, STM32CubeMX error

dgrugur
Associate

dgrugur_0-1737533616351.png

dgrugur_1-1737533666009.png

dgrugur_2-1737533855816.png

dgrugur_3-1737534578043.png

 

Hi,

When I want to generate the code, it says that the STM32CubeMX version is not supported.

Also in the STM32CubeIDE Pinout & Configuration page I don't see "X-CUBE-MCSDK" in the "Middleware and Software Packs" tab.

How can I solve this problem?

Motor Control Workbench in: C:\Program Files (x86)\STMicroelectronics\MC_SDK_6.3.2
STM32CubeMX in: C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX
(It was installed in the locations it automatically selected during installation.
 Both are installed for "all users".)
OS: Windows 10 Pro
OS language: Turkish


 

0 REPLIES 0