cancel
Showing results for 
Search instead for 
Did you mean: 

Motor control workbench generates... empty templates?

tarzan2
Associate III

Hi,

I installed the motor control software (5.4.1) on my computer and start my design for STM32G4. After code generation, I have numerous motor related file in the scr/ and inc/ directories but they are all empty (they only contain the classical ST header). I tried with STM32F3, same issue. I'm using the latest cube MX and libraries.

What's wrong?

3 REPLIES 3
cedric H
ST Employee

Hello,

The issue comes from your repository path of your cubeMX installation.

To fix it, open cubeMX, from Help Menu, select Updater Settings. (no project should be open)

The Repository Folder must end with a final "/" like this :

C:/Users/MyUser/STM32Cube/Repository/

Regards

Cedric

tarzan2
Associate III

This solved the problem, many thanks!

Nicolas

Laurent Ca...
Lead II

The question has been set only to the "STM32 Motor Control" topic (the question is only about the STM32 MC SDK). 

Best regards